TGML Elliptical Chord: <Chord>
Chord defines an elliptical chord. Chord is similar to Pie and Arc.
| Attribute | Type | Description |
|---|---|---|
|
Center |
Point |
The center point of the ellipse. |
|
Fill |
Brush |
Specifies how the interior of the shape is painted. |
|
Opacity |
Double |
A value between "0.0" (transparent) and "1.0" (opaque) |
|
RadiusX |
Double |
The horizontal radius of the ellipse. |
|
RadiusY |
Double |
The vertical radius of the ellipse. |
|
StartAngle |
Double |
Specifies the angle between the x axis and the starting point of the arc. |
|
SweepAngle |
Double |
Specifies the angle between the starting and ending points of the arc. |
|
Stroke |
Brush |
Describes how the line is painted. |
|
StrokeDashArray |
Array of Double |
The pattern of dashes and gaps used to outline shapes: |
|
StrokeWidth |
Double |
The width of the outline of a line. |
| Visibility | Visibility |
Specifies if the element is visible or not. |